TAMPA, FLORIDA & RICHARDSON, TEXAS – December 8, 2014 – Modelithics, Inc., in partnership with TriQuint Semiconductor, has released the latest update to the growing library of high-accuracy non-linear simulation models for TriQuint gallium nitride (GaN) transistors. The TriQuint GaN library, v1.5.0, now contains precision models for 29 of TriQuint's most popular GaN transistors, including the T1G2028536-FL, T1G4012036-FS, and T2G4005528-FS package format transistors, and TGF2023-2-01, TGF2023-2-10, and TGF2954 die format transistors, to name a few.
The TriQuint GaN transistor models have been developed using trusted Modelithics measurements and modeling technology. Each model has been validated over multiple measurements, including multi-bias S-parameters, pulsed IV, single-tone power and load pull at various frequencies. The models have broadband non-linear performance predictability, and offer temperature scaling capability. Advanced design features included with many of the models include scalable operating voltage, control of self-heating effects, and access to intrinsic voltage/current nodes for I/V waveform analysis.
TriQuint's GaN-based solutions offer greater power density, efficiency, frequency range and ruggedness. These qualities enable RF systems to use less electricity, operate with less input voltage and deliver greater RF output power while reducing amplifier size and part counts.
Modelithics President & CEO Larry Dunleavy noted, "This partnership in GaN modeling with TriQuint represents a new format for getting designers tooled with the models they need for design success, with the supplier sponsoring the maintenance, support and distribution of a professionally managed and well documented software library consisting of state-of-the-art non-linear temperature dependent models. We are very pleased to be supporting TriQuint customers in this way."
"TriQuint's partnership with Modelithics will provide designers with precise models for exceptional simulation development," said TriQuint Vice President of IDP Engineering, Brian Balut. "We're excited that production-ready system designs and simulations can now be developed using models of TriQuint's industry leading GaN transistor technology."
The TriQuint GaN models are currently available for FREE download and use by approved TriQuint customers. The model request link can be found at the website address below:
http://www.modelithics.com/mvpTriQuint.asp?comp_id=TriQuint
Each model comes with a model datasheet, which provides detailed information about the model development, features, usage and performance plots. For more information on accessing the new TriQuint GaN Transistor Library, contact Modelithics at 813-866-6335, or email support@modelithics.com.
About Modelithics, Inc.
Modelithics, Inc. (www.modelithics.com) was formed in 2001 to address the industry-wide need for high-accuracy RF and microwave active and passive simulation models for use in Electronic Design Automation (EDA). Current products include the CLR Library™, which contains measurement-based Global Models for a multitude of commercially-available passive component families, the NLD Library™ (non-linear diode models), the NLT Library™ (non-linear transistor models), and the SLC Library ™ (system level component models). Modelithics’ services also address a wide range of custom RF and microwave measurement and modeling needs.
About TriQuint
Founded in 1985, TriQuint Semiconductor (NASDAQ: TQNT) is a leading global provider of innovative RF solutions and foundry services for the world's top communications, defense and aerospace companies. People and organizations around the world need real-time, all-the-time connections; TriQuint products help reduce the cost and increase the performance of connected mobile devices and the networks that deliver critical voice, data and video communications. With the industry's broadest technology portfolio, recognized R&D leadership, and expertise in high-volume manufacturing, TriQuint creates standard and custom products using gallium arsenide (GaAs), gallium nitride (GaN), surface acoustic wave (SAW) and bulk acoustic wave (BAW) technologies. The Company has ISO9001-certified manufacturing facilities in the U.S., production in Costa Rica, and design centers in North America and Germany. For more information, visit www.triquint.com.
Modelithics® is a registered trademark of Modelithics, Inc. CLR Library™, NLD Library™, SLC Library ™, and NLT Library™ are also trademarks of Modelithics, Inc.
TriQuint: Reach Further, Reach Faster™
Modelithics Media Contact:
Lencia Walters
Sales and Marketing Coordinator
Modelithics, Inc.
Tel: +1.813.866.6335
E-mail: lwalters@modelithics.com
TriQuint Media Contact:
Katie Caballero
Marketing Communications Manager
TriQuint Semiconductor, Inc.
Tel: +1.972.994.8546
E-mail: kcaballero@triquint.com