While the majority of the equipment in homes, offices and industries are supplied with 110-480 V AC (alternating current) power, the electronics inside almost always run off a well-regulated DC voltage rail. AC/DC power supplies are therefore almost universally necessary to convert the utility-fed unregulated AC power into stable DC power at specific voltage levels that is appropriate for the end electronics such as 12 V, 24 V, 48 V, 400 V, etc. Qorvo's SiC FETs and Schottky diodes available in 650-1200 V rating and 15-150 mohm on-resistance range are ideal for designing robust, efficient, compact multi-kilowatt power supplies running off the traditional 1-phase or 3-phase AC supply at homes & offices as well as emerging HVDC (high-voltage direct current) supply at industrial facilities & datacenters.
Loading Product Tables
Click on the hot spots in the diagram to see associated products.
AC/DC Power Supply Unit
Click on the hot spots in the diagram to see associated products.
High Voltage DC/DC Power Supply
Click on the hot spots in the diagram to see associated products.
Industrial AC/DC Power Supply