November 29, 2020

    This blog post was first published by United Silicon Carbide (UnitedSiC) which joined the Qorvo family in November 2021. UnitedSiC is a leading manufacturer of silicon carbide (SiC) power semiconductors and expands Qorvo's reach into the fast-growing markets for electric vehicles (EVs), industrial power, circuit protection, renewables and data center power.

    SiC FETs to 650V

    Abstract

    Comparing data sheets for SiC switches can be difficult. SiC MOSFETs can appear to be at an advantage with a lower temperature coefficient of on-resistance, but this is an indicator of higher underlying losses and overall lack of efficiency compared with UnitedSiC FETs.

    Blog

    'Comparisons are odious,' as the proverb goes, first recorded around 1440 in John Lydgate's 'Debate between the horse, goose, and sheep.' Livestock apart, designers of modern power converters have to try to dispassionately compare power switches for their application from a slew of competing claims for 'best performance.' The problem is comparing apple with apples, continuing the farming metaphor, as no single electrical parameter can be said to be better without considering its trade-off with other measures. Switch on-resistance is a good example – you have to compare parts with the same voltage rating, at the manufacturers' recommended gate drive voltage, at the same junction temperature and drain current and in the same package.

    Si-MOSFETs, SiC-MOSFETs and SiC FETS vie for position

    At higher voltages, from a few hundred of volts upwards, Si MOSFETs, SiC MOSFETs and UnitedSiC FETs are vying for position, with datasheets typically giving an RDS(ON) value at a particular voltage rating, junction temperature and gate drive voltage. Part UJ4C075018K4S recently released by UnitedSiC, for example, gives on-resistance values at VGS = 12V and at 25°C to 175°C, all at 20A drain current. From this, you can easily derive a figure for temperature coefficient of RDS(ON) at a given temperature for this part that turns out to be around +70-75% at Tj =125C.

    A champion of 650V SiC MOSFETs might point out that they see a figure of typically +20-25% at Tj =125C for an otherwise similar device. Is that three times better? Firstly, some positive value of temperature coefficient is necessary to force cells in a die to share current without hot-spots and thermal runaway. Similarly, designers rely on the positive value to be able to parallel devices with natural current sharing.

    SiC MOSFET resistance is dominated by its inversion channel

    The lower value for RDS(ON) temperature coefficient of SiC MOSFETs is actually an indication of a deeper effect that is happening; MOSFETs and JFETS are 'single-carrier' devices with electron flow through different regions – substrate, drift layer, JFET regions and channel etc. In a 650V SiC MOSFET, the inversion channel dominates the total resistance, which actually reduces with temperature. Channel resistance is inversely proportional to (number of free carriers x electron inversion layer mobility) and as temperature rises, threshold voltage decreases and the number of free carriers in the channel increases, therefore resistance decreases. This effect is offset by the positive temperature coefficient of the rest of the device regions, namely the JFET, drift layer and substrate resistance, to produce a slight net positive Tc value. In a SiC JFET, there is no inversion channel to offset the positive temperature coefficient of the JFET, drift layer and substrate. Meanwhile, the low voltage Si MOSFET represents only a small portion of the total on-resistance, explaining the higher Tc value than with a SiC MOSFET, but the telling point is that the losses associated with the non-ideal SiC inversion layer are also absent in the SiC FET (Figure 1).

    figure 1
    Figure 1: Typical SiC MOSFET trench construction and a UnitedSiC FET showing absence of lossy SiC MOS inversion channel leading to higher temperature coefficient of on-resistance but lower losses

    SiC FETs have lower overall conduction losses

    The clincher comes when you look at absolute values. As you can see in Figure 2, comparing RDS(ON) for 650/750V devices, the UnitedSiC FET starts at 25°C with around a third of the specific on-resistance of the SiC MOSFET and is still nearly 2x better at 150°C, with about half the consequent conduction losses for the same active die area.

    figure 2
    Figure 2: UnitedSiC FETs have higher Tc of on-resistance but lower absolute values

    The net effect is that there are lower overall conduction losses with a UnitedSiC FET and a healthy positive temperature coefficient of RDS(ON) to ensure effective current sharing between cells and paralleled devices. It clearly pays to make sure comparisons are valid and to understand the mechanisms behind the effects – it can reveal what matters practically: lower overall loss.

     

    Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.

    Explore the Qorvo Blog

    About the Author

    Qorvo Blog Team

    One part technical, one part content, and one part strategic, our small team is dedicated to connecting you with helpful, timely insights from some of the bright minds at Qorvo.