June 1, 2015

    Active antennas are the key to success of 5G networks

    This blog post was first published by Anokiwave, which joined the Qorvo family in March 2024. Anokiwave is a leading supplier of high-performance silicon integrated circuits (ICs) for intelligent, active array antennas for D&A, SATCOM and 5G applications. 

    Active Electronically Scanned Array (AESA) antennas have been used in military phase-array radar systems for many years and are now being deployed in record numbers in a wide range of commercial applications. The highly anticipated rollout of 5G infrastructure is expected to utilize active antenna technologies in both base stations and handsets. Silicon technology is playing a major role in reducing the cost of these new active antennas and offering unprecedented levels of functional integration, allowing the beam steering ASICs to reside within the lattice of the array, resulting in low-profile, planar arrays.

    Silicon-based active antennas will be a key to the success of 5G networks operating at millimeter-wave frequencies. Previously, these frequencies were associated with prohibitively high propagation loss. However, these higher propagation losses can now be overcome by generating highly directional beams with millimeter-wave silicon-based active antennas. The short wavelengths involved allow a high number of radiating elements to be realized in a physically compact area. Additionally, the highly directive beams provide spatial diversity, enabling frequency re-use among separate beams.

    Furthermore, modern silicon technologies work well at millimeter-wave frequencies, making them well-positioned to address upcoming 5G needs. The FCC recently announced that they will recommend at the World Radio Conference 2015 that four new frequency bands (28 GHz, 37 GHz, 39 GHz and 64-71 GHz) be studied for upcoming 5G networks. There is no doubt that silicon ASICs will play a major role in the rollout of these new systems.

    Anokiwave's product portfolio is uniquely positioned to embrace this market with our Silicon Core ICs and System-in-Package solutions for the emerging mmWave active antenna markets.

     

    Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.

    Explore the Qorvo Blog

    About the Author

    Qorvo Blog Team

    One part technical, one part content, and one part strategic, our small team is dedicated to connecting you with helpful, timely insights from some of the bright minds at Qorvo.