November 14, 2017
This
is the first of a two-part blog series that looks at the design challenges for
Wi-Fi front-end designs. Part 2 examines coexistence and
interference.
For wireless access points or customer premises
equipment (CPE), it can be hard to fully account for thermal management
and the parameters affected by it prior to FCC certification. To save yourself
the headaches of last-minute changes due to interference, coexistence or RF
front-end (RFFE) linearity, be sure to design using component thermal
parameters in mind. This blog post explains the biggest thermal challenges
facing Wi-Fi front-end designs.
On average, today’s households have 12 clients or Internet of Things (IoT) products communicating with each other, but these numbers will increase in coming years. Intel believes the number of household clients will increase to 50 in 2020, while Gartner predicts 20.4 billion connected things will be used worldwide by 2020.
In today’s wireless homes, communication operators and retailers have typically offered one large wireless router, using raw power to achieve coverage across the entire home. But with the sharp increase of household devices and the IoT, smart homes are pushing the capabilities of the single-router model.
As a result, new application models are evolving. Consumers are finding that placing more routers, or nodes, in the home helps service more clients and data backhaul to the home router/modem. This mesh (or distributed Wi-Fi) network model ensures wireless capability across a home using some techniques that are already present in office headquarters, hospitals and college campuses via enterprise-level systems.
Related Blog Post: How Distributed Wi-Fi Enables Connected Smart Homes
It’s no surprise that the RF complexity within the access point increases because of this mesh networking model and as devices integrate more standards and capabilities.
The IoT brings several challenges:
Block diagrams of older vs. new access points highlight just how complex the RFFE design is now.
All these changes in the Wi-Fi front-end design increase the number of RF chains, contributing to the overall heat within the access point. This increase in unit temperature also increases the RF tuning challenges, especially when the size of the box is the same or even smaller.
In the Wi-Fi world, one of the most critical design challenges engineers
need to address is product temperature. In today’s products, components
are subject to average temperatures of 60°C or greater, while sitting in a
room temperature environment of 25°C. It’s important to consider
this fact early on in a design, to help minimize redesign issues or additional
costs.
Temperature affects three RFFE components:
Let’s examine the heat challenges and Wi-Fi design considerations for
each category.
In the Wi-Fi world, one of the most critical design challenges engineers need to address is product temperature.
Engineers often balance between linearity, power output and efficiency in each of the RF chains. Using optimized, highly linear power amplifiers or front-end modules (FEMs) optimizes system efficiencies, creating less overall heat. It also reduces processing inefficiencies.
RF engineers should also consider several Wi-Fi design trends that affect power amplifiers:
In the switch, insertion loss can also generate excess heat. When insertion loss increases and signal strength is lowered, the PA works harder to compensate and push higher outputs, which degrades efficiency. And less efficiency means more heat from the device. Using high-linearity, low-loss switches keeps the insertion loss within specifications across the entire band.
Receive throughput is highly dependent on the LNA gain and noise figure.
Although the LNA doesn’t contribute significantly to heat generation,
the effect of heat on the LNA can drastically affect throughput. Heat degrades
the noise figure, and depending on the circuit design and choice of wafer
technology, the compensation for this can lead a designer to a specific
solution.
RF filters drift to the left or the right due to changes in temperature, as shown in the following SAW vs. BAW figure. These shifts can cause high insertion loss on the band edges, which could cause a low gain or POUT response from the RFFE. If the filter drifts too much (as shown in the SAW figure), then the PA pushes more power output to compensate for the insertion loss. This increases current and decreases system efficiency.
Using filters with high insertion loss can decrease linearity and increase the RF chain POUT. One big advantage of Qorvo’s LowDrift™ bulk acoustic wave (BAW) filters is their stability over temperature shifts. Diplexers, bandpass filters and coexistence filters that use BAW technology with lower temperature drift help mitigate insertion loss, and lead to good product thermals.
Read More Design Tips: Resolving Interference in a Crowded Wi-Fi Environment Using BAW Filters
Watch this detailed "Chalk Talk" video to learn more about Qorvo's Wi-Fi connectivity solutions (37:56).
Heat can degrade overall system performance (such as throughput, range and interference resolution). As a result, it’s important to design systems by choosing RFFE components that mitigate the heat. In the transmit chain, the focus should be on balancing link budget needs such as system linear power.
As devices move from 802.11ac to 802.11ax capability, product manufacturers must focus on using more efficient components. Qorvo challenges its design teams to increase linear power without increasing power dissipation — designing higher throughput devices with the same power consumption as previous generations. One example is the QPF4528, an 802.11ax 5 GHz FEM that transmits linear powers achieving -47 dB EVM — above the current QPF4538 FEM, an 802.11ac 5 GHz FEM that achieves ‑43 dB EVM with the lower maximum power dissipation.
Another product that integrates all the aspects of heat mitigation is Qorvo’s QPF7200, a fully integrated front-end module (iFEM) that reduces weight and design complexity while also decreasing system heat. The QPF7200 module:
With so many radios and RF chains squeezed together, it’s important to partner with an RF supplier that helps you achieve low power dissipation and linear power budgets simultaneously.
Although many systems are designed and modeled at room temperature, ask yourself how it will operate at 60-70°C (140-158°F) when the device is operating. Don’t wait until FCC certification time to find out.
Check out Part 2 in our series, where we address Wi-Fi design challenges around wireless interference/coexistence, and smart tips to overcome them.
Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.