August 23, 2017
Wi-Fi
initially was 1x1 — a single stream, with a single client talking to a
router — but it has evolved into an 8x8 MIMO (multiple input/multiple
output) solution where multiple clients talk to a router at the same time. The
current Wi-Fi standard, 802.11ac (now called Wi‑Fi 5), was fully released in late 2013, and
it works very well in a home environment. But as with previous Wi-Fi
standards, it may reach its limits around 2022 when there could be 50 nodes in
a home, per the Organisation
for Economic Co-operation and Development (OECD).
802.11ax (now called Wi‑Fi 6) is the next evolution in the IEEE 802.11 Wi-Fi standard and will become prevalent in very dense environments, such as urban apartment complexes, college campuses, concert venues, or sports stadiums, where many clients will access the internet over Wi‑Fi. The IEEE standard currently is in development and expected to be publicly released in 2019.
Let's take a look at five key things you need to know about 802.11ax (Wi‑Fi 6) and the next generation of Wi‑Fi.
See the table below for additional differences between 802.11ac and 802.11ax.
Glossary of Terms
6.9 Gbps just isn't possible in a home or public Wi-Fi network. We will never see the theoretical speeds listed on the box of a router on the shelves at Best Buy, Walmart or other big-box stores.
The most limiting factor at home is the connection from the internet provider — the pipe coming into the home for internet access. If a router can support 1.6 Gbps but the connection to the home is only 100 Mbps, a client will never realize that higher speed for downloads from the wide area network (WAN).
The data stream into a home and the access point will establish the initial internet bandwidth benchmark. From there, other factors can slow the network speed:
A Wi‑Fi 6 access point will provide a more efficient environment, mitigating the problems of Wi-Fi overhead — in other words, the fixed "cost" associated with the communication that isn’t a part of the data transmission. 11ax will attack the overhead differently, scheduling when a device operates and handling the information and clients more efficiently.
Additionally, advanced filtering techniques enable better coexistence and bandedge performance. This has two effects:
Altogether, improved efficiency and filtering will help 802.11ax have
faster speeds than 11ac.
802.11a up to 802.11ac use OFDM, or orthogonal frequency-division multiplexing, to deliver Wi-Fi data packets. Under OFDM, a device uses a fixed 20 MHz or 40 MHz of bandwidth to deliver the packets, regardless of whether it's transmitting video or just sending a simple text message over a Wi-Fi network.
Wi‑Fi 6 (802.11ax), however, uses OFDMA, or orthogonal frequency-division multiple access, which allows resource units (RUs) that divide the bandwidth according to the needs of the client and provides multiple individuals the same user experience at faster speeds.
A simple analogy using trucks can illustrate the difference, as shown in the image below. Each truck is hauling a payload, or user data — one surfing the web, another uploading video from a soccer game and a third sending a text message, for instance. Under OFDM, a device had to use three trucks of the same size to send the data, regardless of how empty or full each truck was. In other words, OFDM inefficiently uses the bandwidth, leaving a lot of empty space. OFDMA, in contrast, allows a device to fill an entire truck with RUs (i.e., data) — a payload delivery model that uses the bandwidth much more efficiently.
With 1024 QAM modulation, there are more bits per symbol — 10 bits per symbol versus 8 bits in 256 QAM. More bits equals more data, and the payload delivery of data is more efficient — like having a bigger truck.
At the same time, OFDMA decreases the spaces between the subcarriers, packing even more resource units into the truck, so to speak.
But as the data rate increases, error vector magnitude (EVM) on the RF front-end becomes paramount. With 1024 subcarriers in Wi‑Fi 6 (802.11ax), the constellation is flooded and so dense that the system must distinguish one of the points from another. It takes a very sophisticated system to decode (or demodulate) these constellation points, and it requires devices to have better EVM.
Wi‑Fi 5 (802.11ac) requires -35 dB PA EVM, while Wi‑Fi 6
(11ax) requires -47 dB PA EVM. Higher modulation schemes require better
EVM so that a device can attain the higher efficiencies of the data
packet.
As already said, Wi‑Fi 6 (802.11ax) pushes the EVM requirements down to -47 dB, but access points and clients still have to meet the same spec. There’s no difference.
Power levels can be very different, though. Access points or customer premises
equipment (CPE) typically operate at much higher power than a
client — 24 dBm versus 14-20 dBm for a mobile handset.
Ultimately, a lot more power means a lot more heat
that has to be dissipated, so a connectivity solution may require a more
stringent thermal requirement compared to a mobile solution.
It's important to realize that the Wi‑Fi 6 (802.11ax) specification
is still in flux and won't be finalized for some time. Stay tuned for more
insights as the next standard of Wi-Fi continues to evolve.
Read more Wi-Fi design tips:
Wi-Fi 6 is making the connected home of tomorrow a reality. See how Qorvo's "pod in every room" concept brings this vision to life. Watch Our Video >
Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.