December 13, 2017

This article first appeared on Network World, by IDG contributor Brent Dietz.

Tesla’s “Maximum Plaid” speed mode rockets its new Roadster from 0-60 in 1.9 seconds. If you think that’s fast, go ahead and Google “5G.”

5G is Plaid for cellular networking – a next-generation mobile network that promises not only ten-times the available spectrum, for ten-times the download speeds, but across ten-times the devices and with a fraction of the latency.

The move from 1Gbps to 10Gbps speeds will support bandwidth-intensive applications like high-definition video and virtual reality, and near real-time connections will enable ultra-low latency applications like autonomous cars, remote surgery and specialized applications within the Internet of Things (IoT).

5G is impressive, but – spoiler alert – it isn’t entirely new. The road to 5G runs through 4G wireless infrastructure, and improvements to 4G technologies like carrier aggregation, small cells, massive multiple-input and multiple-output (MIMO) and beamforming will satisfy our need for 5G speed.
 

Speed

Carrier Aggregation

IDC forecasts that by 2025 the global datasphere will grow to 163 zettabytes. For the folks at home, that’s 163 trillion gigabytes. Much of this will be mobile data, transmitted in real-time between phones and IoT devices.

As demand for mobile data increases, mobile carriers and manufacturers face a conundrum. There is a finite amount of radio frequency spectrum at any given time, but they must increase capacity and offer faster data speeds to meet user demand. The key is squeezing the most out of existing RF spectrum – and for that, there’s carrier aggregation (CA).

CA is a technique that combines multiple carrier signals – or “channels” – to increase network performance. As consumers, we love CA, because we hate buffering. CA accelerates downloads and uploads, allowing cellular networks to move more data, faster.

Gamers and Instagram influencers, rejoice!

CA is already used to combine multiple 4G LTE-Advanced frequency bands. As we approach 5G, cellular service providers will seek to squeeze even more bandwidth out of existing spectrum by combining as many as five channels.

Small Cells

Cellular base stations connected to cell towers carry signals over the river and through the woods to the dinner table at grandma’s house. Because 5G builds on the 4G foundation, carriers can simply upgrade these towers to support higher 5G frequencies, like 28GHz and 39GHz.

But there’s a catch. These millimeter wave (mmWave) frequencies cannot penetrate walls or buildings. Thick walls, frame and cement impede mmWave signals, turning downtown into a dead zone. Plus, being far from a base station is a drag – on your battery life, that is.

This is where small cells come in: mini base stations that act as a relay team to transmit around objects, improve battery life and deliver an extra boost in densely populated areas, like sports stadiums, airports and urban centers. Small cells also help service providers avoid satellite dish syndrome, eliminating expensive rooftop systems while extending coverage.

Massive MIMO

I say, “massive,” you say, “tiny antennas!”

Maybe not, unless you’re an RF engineer familiar with massive MIMO. Massive MIMO is a fancy term for equipping cell towers with more antennas to extend network capacity without requiring more spectrum. Sound familiar?

We’re not talking an antenna or two. Massive MIMO systems have ten times more antennas than traditional MIMO systems to connect to multiple devices at once. At Mobile World Congress this year, Nokia and Sprint demonstrated massive MIMO technology with 64 antennas each for uplink and downlink. According to CIO, this increased capacity by as much as eight times for downloads and as much as five times for uploads.

Massive MIMO has been called the backbone of 5G. Without it, operators could not handle the bandwidth and capacity requirements for the next-generation network. Tiny antennas, massive impact.

Beamforming

… but tiny antennas also cause massive interference problems.

Enter beamforming, and no, that’s not a teleporter. Beamforming technology drives signals directly to the point of use. We see this with many new Wi-Fi routers, where beamforming is used to focus the Wi-Fi signal and improve signal strength and range.

Beamforming is used similiarly in base stations. With this technology, base station antennas focus data streams as they leave the tower, improving speed and reliability for consumer devices.

So, whether you’re video chatting across the country or sharing cat memes across the table, take a moment to thank these 4G technologies for the speed.

Oh, and buckle your seatbelts. We’re going to Plaid.

 

Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.

Brent Dietz

About the Author

Brent Dietz
Director of Corporate Communications

Brent has seen a lot of engineering and technology during 30+ years in the tech industry. His primary role is making geek-speak understandable to the non-geek public, reporters and nontechnical analysts. It's challenging — simplifying without distorting — and it helps to have a sense of humor. Brent does, which he shares with readers from time to time.

  • Innovation
    5G The Future of RF

    Qorvo is the standard setter – participating in standards bodies and partnering with wireless carriers – to define 5G RF for the future.

  • Applications
    Carrier Aggregation

    Our high-performance RF solutions solve network congestion by enabling carrier aggregation.

  • Applications
    Small Cells

    Qorvo has an extensive product portfolio supporting small cell infrastructure.

  • Applications
    Internet of Things

    Qorvo's innovative portfolio enables the smart home, smart energy and other IoT applications.