QPB3810 and QPB9362 press image
    Download full size image

    Greensboro, NC, June 8, 2023 – Qorvo® (Nasdaq: QRVO), a leading global provider of connectivity and power solutions, today expanded its family of products for 5G base stations. Qorvo’s QPB3810 is a gallium nitride (GaN) based power amplifier module (PAM) with integrated bias control for 5G massive MIMO (mMIMO) applications. Qorvo’s new QPB9362 is a highly integrated front-end low noise amplifier (LNA) module targeting 5G TDD systems. The devices extend Qorvo’s broad product portfolio supporting mMIMO applications and are key building blocks in a new RF front-end reference design that accelerates adoption of mMIMO systems.

    Anthony Collins, Director 5G Radio and RF Ecosystem, AMD, said, “We are pleased to continue our close cooperation with Qorvo to enable high-performance 5G solutions using industry-leading AMD Zynq UltraScale RFSoC DFE devices. Collaborating to deliver proven and optimized reference designs to our mutual customers is key to reducing risk and enabling faster time to market for their radio products.”

    QPB3810 is a 48V, 8-watt average power PAM covering the 3.4 - 3.8 GHz band, and is the first commercially released GaN-based module with an integrated bias controller factory programmed to set the optimal bias points of the Doherty PAM. The controller includes a temperature sensor that automatically adjusts bias over temperature and includes an enable pin for fast TDD switching. The QPB3810 is available in a compact 12 mm x 8 mm SMT package, offering a much smaller footprint than traditional discrete component solutions. Like Qorvo’s other PAM products, the QPB3810 requires minimal external circuitry. The linearity of the QPB3810 has been validated to exceed 5G requirements over 400 MHz instantaneous bandwidth using the AMD Zynq™ Ultrascale+™ RFSoC DFE Adaptive Radio SoC and Digital Pre-Distortion IP.

    The QPB9362 is targeted for 5G wireless infrastructure applications configured for TDD-based mMIMO architectures. The switch LNA module integrates an LNA with a high-power handling switch which can be used as a failsafe path to termination when a radio is transmitting. The QPB9362 provides 34.5 dB of gain with 1.1 dB typical noise figure over the entire operating frequency band in the receiving mode. LNA power-down mode is available via a transmit/receive control pin on the module. It is packaged in a RoHS-compliant, compact 5 mm x 3 mm LGA package.

    Tuan Nguyen, product line director for the Infrastructure Solutions business at Qorvo, said, "Qorvo's 5G modules provide optimal solutions that minimize cost, maximize performance and increase capacity for mMIMO designs. These two modules support the continued expansion of 5G technology around the globe with much greater integration at the board level and exemplify our focus on ease of use and efficiency."

    The QPB3810 and QPB9362 are included in a full RF front-end reference design for 5G mMIMO applications now available from Qorvo. This small form factor reference design provides a transmit/receive RF solution from the baseband front-end to the antenna filter. The transmit lineup includes the QPA9122M wideband high linearity pre-driver, the QPB3810, a directional coupler for DPD observation, and a circulator. The receive path includes the QPB9362.

    Learn more about Qorvo 5G Infrastructure solutions.

    Connect with us at IMS (#IMS2023), June 11-16, in San Diego, California. For more information about Qorvo's solutions, announcements and meeting inquiries, visit our Qorvo IMS 2023 page.

    About Qorvo
    Qorvo (Nasdaq: QRVO) supplies innovative semiconductor solutions that make a better world possible. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including consumer electronics, smart home/IoT, automotive, EVs, battery-powered appliances, network infrastructure, healthcare and aerospace/defense. Visit www.qorvo.com to learn how our diverse and innovative team is helping connect, protect and power our planet.

    Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries. All other trademarks are the property of their respective owners.

    Contact:
    Cindy Warschauer
    Strategic Marcom Manager
    cindy.warschauer@qorvo.com
    +1-870-688-3974

    This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions, and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under U.S. federal securities laws. Our business is subject to numerous risks and uncertainties, including those relating to fluctuations in our operating results; our substantial dependence on developing new products and achieving design wins; our dependence on several large customers for a substantial portion of our revenue; the COVID-19 pandemic materially and adversely affecting our financial condition and results of operations; a loss of revenue if defense and aerospace contracts are canceled or delayed; our dependence on third parties; risks related to sales through distributors; risks associated with the operation of our manufacturing facilities; business disruptions; poor manufacturing yields; increased inventory risks and costs due to timing of customer forecasts; our inability to effectively manage or maintain evolving relationships with platform providers; our ability to continue to innovate in a very competitive industry; underutilization of manufacturing facilities as a result of industry overcapacity; unfavorable changes in interest rates, pricing of certain precious metals, utility rates and foreign currency exchange rates; our acquisitions and other strategic investments failing to achieve financial or strategic objectives; our ability to attract, retain and motivate key employees; warranty claims, product recalls and product liability; changes in our effective tax rate; changes in the favorable tax status of certain of our subsidiaries; enactment of international or domestic tax legislation, or changes in regulatory guidance; risks associated with environmental, health and safety regulations and climate change; risks from international sales and operations; economic regulation in China; changes in government trade policies, including imposition of tariffs and export restrictions; we may not be able to generate sufficient cash to service all of our debt; restrictions imposed by the agreements governing our debt; our reliance on our intellectual property portfolio; claims of infringement of third-party intellectual property rights; security breaches and other similar disruptions compromising our information; theft, loss or misuse of personal data by or about our employees, customers or third parties; provisions in our governing documents and Delaware law may discourage takeovers and business combinations that our stockholders might consider to be in their best interests; and volatility in the price of our common stock. These and other risks and uncertainties, which are described in more detail in Qorvo's most recent Annual Report on Form 10-K and in other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.