DALLAS, TX – October 24, 2018 – The ACT88325 and ACT88326 PMICs are integrated field programmable ActivePMU™ power management units, also referred to as PMICs (Power Management ICs). The products are highly flexible with non-volatile memory and come pre-programmed and can be field programmed via I2C or via GPIOs for multiple applications.
The ACT88325 powers up based on the preconfigured startup sequence as soon as power is applied to the input pin, whereas ACT88326 implements a Push Button Startup that relies on a customer's interaction with, for example a portable application like an Action Camera, Video Doorbell, Body Camera or other handheld applications.
"Low external component count, extremely small WLCSP package and high configurability significantly speeds time to market and reduces PCB size and BOM cost" says David Briggs, VP and General Manager of Power Solutions at Active-Semi. "The ACT88325 and ACT88326 are a great addition to our lineup and are specifically designed for the highest power density in SSDs and the ACT88326 for portable applications, where everyone wants smaller and lighter, with the push button start."
The core of the devices includes 3 DC/DC step down converters using integrated power FETs, and 2 low-dropout regulators (LDOs). The buck converter and LDO can be reconfigured as a bypass switch and an additional high-power load switch controller is included.
The ACT88325 and ACT88326 PMICs are available in a 2.8 x 3 mm 36 ball WLCSP package with optimized pinout for easy PCB routing. The pinout is optimized to implement PTH (Plated-Through Hole) under the package to optimize layout efficiency and reduce the required PCB layers for routing.
For more information visit:
https://www.qorvo.com/products/p/ACT88325
https://www.qorvo.com/products/p/ACT88326
Please visit www.qorvo.com/how-to-buy for additional contact and purchasing information.
About Qorvo
Qorvo (Nasdaq: QRVO) makes a better world possible by providing innovative Radio Frequency (RF) solutions at the center of connectivity. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including advanced wireless devices, wired and wireless networks and defense radar and communications. We also leverage unique competitive strengths to advance 5G networks, cloud computing, the Internet of Things, and other emerging applications that expand the global framework interconnecting people, places and things. Visit www.qorvo.com to learn how Qorvo connects the world.
Qorvo is a registered trademark of Qorvo, Inc. in the U.S. and in other countries. All other trademarks are the property of their respective owners.
Media Contact: |