Headquarters: Finland
Region(s) Served: EMEA
CoreIoT is one of the world's most valued and fastest growing Antenna and RF passive component solution company that has spread its wings to many nations and has clients around the globe. We partner with companies for their products that needs superior wireless performances with ingenious antenna solutions in any complex environments and provide them with best off-the-shelf or customized antenna based on their need and depending on their connectivity issues.
We stand unique within the market with a group of talented and client-centric team that uses a consultative approach, from years of experience working in companies like Nokia and Microsoft Mobile Ltd. We implement cutting-edge Antenna simulation software and state-of-art high precision tools to deliver the best antenna performance based on our client's needs.
The unique trait of our products is that we can tune the frequency of these off-the-shelf antennas based on the client's devices and its capacity. We are further venturing into developing antennas to varied set of newly spurring IoT devices of the recent times. We also design, simulate and test antennas based on our client's needs, tune them depending on the frequency that is best suitable for the device and establish a smooth integrated working accordance. Some of our other services are Multi-antenna isolation measurement, Transmission line design & PCB layout file review and RF material characterization.
We have the best team of efficient engineers working alongside each other to take our mission into a reality and carry forward our vision with great enthusiasm and perseverance. Their team spirit and coordination has ensued both them and our company a great zeal of knowledge along with an urge to comprehend any spurring technological invention related to the field and implement them in the passion for their work.
UWB SMD Chip Antenna
CoreIoT's Ultra-Wideband SMD Chip Antenna has been specifically designed for Europe and USA UWB Applications at the operating range within 5.98 - 8.237GHz, with dimensions 6.2 mm x 4.85 mm x 1.55 mm.
UWB chip antenna is a highly efficient, compact form factor UWB antenna. It is mounted to a PCB via a standard SMT reflow process.
UWB antenna return loss is better than -10 dB and efficiency above 75% across the 5.98 - 8.237GHz UWB band.
Dual Band WLAN
CoreIoT Dual Band WLAN has been specifically designed for Bluetooth and Wi-Fi applications at the operating range within 2400 - 2550 MHz & 4900 - 5900 MHz, with a space requirement of 18.4 x 17.4 x 0.8 mm.
Frequency (MHz) | 2400 - 2484 | 4900 - 5850 |
VSWR | 1.92:1 | ≤ 3:1 |
Return Loss (dB) | ≥ 10.52 | ≥ 6.05 |
Peak Gain (dBi) | ≥ 2.2 | ≥ 2.12 |
Efficiency (%) | ≥ 68 | ≥ 43 |
LTE Chip Antenna
CoreIoT LTE chip antenna is designed to cover the full cellular 2G / 3G/ GSM / 4G /LTE bands, frequencies 698 - 960 MHz & 1710 - 2690 MHz. Antenna delivers excellent performance and is fully compatible with SMT processes which decreases the assembly cost and improve device's quality and consistency.