Headquarters: U.S.

    Region(s) Served: APAC, EMEA, Latin America, North America

    Ambient Photonics was founded in 2019 in California to bring low light energy harvesting technology to mass scale. With a focus on IoT applications, the company aims to inspire a new generation of connected devices with endless power.

    Our technology is rooted in the simplicity of nature, but it doesn't rely on the power of the sun. Instead, we looked at how photosynthesis works and turned the science behind it into a bright new idea: use the low-level ambient light that surrounds us everywhere to generate power.

    The company has developed a first-of-its-kind low light energy harvesting photovoltaic (PV) technology that generates more than three times the power of conventional indoor PV technologies from a broader spectrum of indoor and outdoor ambient light. This chemistry breakthrough enables revolutionary advances in device design, function, performance, sustainability, reliability and consumer experience.

    Unlike high performance solar photovoltaic technologies of the past, these innovations are cost compatible with today's mass scale technologies. Ambient employs a novel industrial solar printing technology to coat its proprietary chemistry on thin, durable glass substrates — producing photovoltaic cells of virtually any size and shape. This flexibility empowers industrial designers, allowing them to embed Ambient's cells into a variety of product shapes and structures.

    Products

    Inner Solar Cell

    High efficiency indoor light harvesting

    Return to Ultra-Wideband Partners page