Headquarters: Spain

    Region(s) Served: EMEA

    A Blue Thing In The Cloud is an European electronics engineering company. It was founded by Javier Longares, electronics engineer with 20 years of professional experience designing a wide-range of electronic products. The company consists of a high-skilled and top-talented team working in permanent positions in the company, who will willingly collaborate in the success of every project.

    The company is in charge of offering development and consultancy services like PCB Design and Firmware Development.

    It is specialized in the development of BLE and IoT devices, at the point of referring these technologies in our company name. We are also experts in RTLS with the UWB technology offered by Qorvo.

    A Blue Thing In The Cloud also offers related services like device conception, low power consumption analysis, static analysis over existing code, reducing technical debt, and ensuring firmware compliancy with ISO and IEC standards.

    It also sells firmware libraries, as a product family called BlueStack.

    BlueStack are firmware libraries intended to reduce the time-to-market of the new products of our clients. There are BlueStacks for IMUs-based accelerometers, BLE, cryptography (including Secure Channel Protocol 03), and UWB-based RTLS.

    BlueStacks can be ported to any microcontroller. Two versions are always offered. A free demo version with some limited functionality and including some pre-built libraries, and a Pro version, where the client will have the full source code of the library, and will be able to modify or customize it specifically for its product application.

    Products & Services

    BlueStackUWB (Demo)

    Free demo version of the BlueStackUWB firmware stack.

    • Firmware compatible with DWM1000, DWM1001C and DWM1004C, to read and write its registers.
    • Compatible with ESP32, NRF52 and STNM32 microcontrollers, and can be easily ported to any microcontroller by building a new Hardware Abstraction Layer.
    • It implements a version of the Two-Way Ranging Algorithm, with firmware for both initiator and anchor. Allowing calibration and distance calculations.
    • It implements a demonstration of a Real Time Location System based on the Two-Way Ranging Algorithm with a maximum of 3 anchors.

    Some code libraries are provided as pre-built libraries.

    BlueStackUWB (Demo)

    BlueStackUWB (Pro)

    Full version of the BlueStackUWB firmware stack.

    • Firmware compatible with DWM1000, DWM1001C and DWM1004C, to read and write its registers.
    • Compatible with ESP32, NRF52 and STNM32 microcontrollers, and can be easily ported to any microcontroller by building a new Hardware Abstraction Layer.
    • It implements a version of the Two-Way Ranging Algorithm, with firmware for both initiator and anchor. Allowing calibration and distance calculations.
    • It implements a demonstration of a Real Time Location System based on the Two-Way Ranging Algorithm with no maximum of anchors.

    All the source code of the stack is provided, so it can be customized by the end-user.

    BlueStackUWB (Pro)

    PCB Design & Firmware Development

    A Blue Thing In The Cloud is a company specialized in offering PCB Design and Firmware development services.

    The name of the company comes from the technologies where we have more expertise: the design of devices with BLE and IoT functionalities.

    From the device conception, to the manufacturing of a physical product ready to be sold, including firmware static analysis, and technical debt reduction, your company will never walk alone.

    PCB Design & Firmware Development

    Return to Ultra-Wideband Partners page