August 2, 2022

    It’s no secret that powering up and down GaN power amplifiers (PAs) in some designs can be challenging because GaN PAs demand specific bias sequencing. If it’s not done properly, there’s a risk of component damage. Managing the sequencing procedure is crucial. The good news: this task just got easier.

    Our new video demonstrates how customers using GaN PAs can use the Qorvo ACT41000 power management module to help efficiently power-up and power-down those devices. This can help achieve the performance customers are looking for and simplify the GaN bias procedure.

    After setting up the PA using the GUI of the ACT41000, it automatically adjusts the power-up and power-down sequence of the GaN PA while optimizing the PA quiescent bias for optimal system performance (see Figure 1). This simplifies the RF PA system design, making it more cost-effective and easier to use. Because of the ability to autotune, the ACT41000 removes the need for external digital-to-analog converters (DAC) and current sense amplifiers. Therefore, your system is not only easier to design and smaller, but it lowers the overall bill of material costs by reducing the number of components.


    Watch the video to see how customers using GaN PAs can use the Qorvo ACT41000 power management module to help efficiently power-up and power-down those devices.
    (video length: 3:40 minutes)

    Tri-Band Wi-Fi Frequency Bands for 2.4 GHz and 5 GHz
    Figure 1: Block diagram design of ACT41000 powering the QPA2211.

    The ACT41000 comes with an evaluation platform and GUI that offers help in fine-tuning bias, as shown in Figure 2. The auto-tuning feature also aids in optimizing bias performance of the GaN PA during equipment aging or temperature fluctuations. As the GaN PA sees environmental or aging changes, the ACT41000 fine-tunes the device voltage and current values to adjust for optimal performance settings defined in the GUI. This is very important in applications like 5G towers where conditions are hot during the day and cooler at night. Auto-tuning bias helps optimize performance during these fluctuations. This allows engineers to automate the design, which makes it easier and enables them to offer their customers more reliable optimized solutions.

    Tri-Band Wi-Fi Frequency Bands for 2.4 GHz and 5 GHz
    Figure 2: GUI used to set up the ACT41000.

    The ACT41000 can operate from an input voltage between 4.5 to 40 volts and can generate a regulated adjustable output voltage up to 34 volts at 4 amps. It can do this in small steps of 12.5 millivolts. Additionally, it integrates the power MOSFETs and current DAC, allowing the device to precisely detect the GaN PAs quiescent drain current. This benefit, along with its built-in configurability, will enable it to bias a variety of GaN PAs across many markets like satellite communications, cellular 5G, radar and many more, as shown in Figure 3.

    Tri-Band Wi-Fi Frequency Bands for 2.4 GHz and 5 GHz
    Figure 3: Block diagram of ACT41000 and GaN PA applications that can be applied.

    Using power management devices like the ACT41000 for GaN PA biasing can resolve the diverse challenges of maintaining the performance of your system. To learn more about how the ACT41000 can be used in GaN PA applications, visit Qorvo’s short tutorial video.

    For more resources focused on tackling complex design challenges, visit the Qorvo Design Hub for a rich assortment of videos, blog articles, white papers, tools and more.

     

    Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.

    Explore the Qorvo Blog

    About the Author

    Qorvo Blog Team

    One part technical, one part content, and one part strategic, our small team is dedicated to connecting you with helpful, timely insights from some of the bright minds at Qorvo.