September 23, 2024

    Try to think of a time when you didn’t use an electric motor. From the ceiling fan in your home to the windows in your car to delicate surgical instruments in a hospital—electric motors are a cornerstone of modern technology, consuming more than half of the world’s electricity. Increasing energy efficiency can significantly reduce global electricity demand—the best-performing motors with smart control. Our white paper offers a closer look.

    Qorvo’s white paper, "Design Challenges and Considerations for Brushless DC Motors and Their Drives," examines the challenges and benefits associated with Brushless DC (BLDC) motors.

    Motors have been used for the past 100 to 150 years. At first, they were incredibly simple: You connected them to a power source, and they would work. However, because of the demands placed on them, this wasn't the most efficient way of performing a motorized task. Motors and the devices controlling them had to become much more sophisticated.

    For the past 12 years, Qorvo has been integrating motor control into a single chip to make the application much smaller, which can also save on cost. Some applications, such as a battery-operated drill, need a small space footprint, which means they need to fit the palm of your hand. This requires many design challenges, but meeting those challenges can yield many benefits.

    Design Challenges

      Initial Costs
    • Higher upfront costs for BLDC motors and their drives compared to traditional motors.
    • Integration of advanced control electronics adds to the initial investment.
      Complex Control Systems
    • Need for sophisticated control algorithms to optimize performance.
    • Requires significant processing power and advanced software for optimal operation.
      Motor Selection
    • Choosing the right motor type based on application requirements (e.g., continuous vs. intermittent torque and speed).
    • Ensuring compatibility with existing systems and performance expectations.
      Sensor Integration
    • Deciding on the type and placement of sensors for accurate rotor position detection.
    • Balancing cost and performance with different sensing technologies (e.g., Hall effect sensors and optical encoders).
      Heat Management
    • Effective dissipation of heat generated by power electronics and motor operation.
    • Maintaining performance and longevity under varying operational conditions.

    Benefits of BLDC Motors

      High Efficiency
    • Potentially over 96% efficiency, leading to significant energy savings.
    • Lower lifecycle costs due to reduced electricity consumption.
      Long Lifespan
    • Minimal maintenance requirements as there are no brushes to wear out.
    • Durability and reliability in various applications.
      Compact and Lightweight
    • Higher power density allows for more compact motor designs.
    • Ideal for applications where space and weight are critical factors.
      Enhanced Performance
    • Precise control over speed and torque with advanced drive electronics.
    • Smooth operation and reduced torque ripple, especially with sinusoidal commutation.
      Versatile Applications
    • Suitable for a wide range of applications, from small handheld tools to large industrial machines.
    • Flexibility in operation with both battery-powered and main-powered systems.

    Qorvo BLDC Motor Control Solutions

    To use all of this capability, the motor's different electrical parameters must be controlled. This requires a lot of handholding, and that is where the motor controller comes into play. In this case, the one Qorvo provides has a microcontroller that houses the required intelligence.

    Qorvo offers integrated solutions to address the challenges of BLDC motor control. Their PAC5xxx series Power Application Controller™ (PAC) integrates all necessary functions for BLDC motor control:

    • High Integration: Combines three-phase gate drivers, power management, analog front end, multiple communication interfaces and sensor interfaces.

    • Configurable and Updateable: Allows for field updates and auto-tuning for specific motors. Comprehensive Protection: Includes over-current, under-voltage, over-voltage and over-temperature protections

     

    • Space and Cost Efficiency: Minimizes board space requirement, as well as component count, reducing BOM and assembly costs.

     

    The PAC series simplifies the implementation of BLDC motors, ensuring high performance, efficiency and reliability across various applications.

    For safety, we created a new line of drivers with two features. We moved these safety measures from software to hardware. Now, you have a hardware implementation that allows the motor to be stopped quickly and the power stage to be disabled with hardware instead of firmware. This ensures potential firmware glitches cannot interfere with and compromise safety. Allowing for redundancy increases safety on some power tools, such as chainsaws, for which safety is paramount.

    Despite their initial cost and complexity, BLDC motors offer unmatched efficiency, longevity and performance benefits. By overcoming design challenges with integrated control solutions like Qorvo’s PAC series, industries can achieve substantial energy savings and operational improvements.

    Learn more in the white paper "Design Challenges and Considerations for Brushless DC Motors and Their Drives."

     

    Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.

    Explore the Qorvo Blog

    About the Author

    Qorvo Blog Team

    One part technical, one part content, and one part strategic, our small team is dedicated to connecting you with helpful, timely insights from some of the bright minds at Qorvo.