March 22, 2018

    Internet of ThingsThis blog is the fourth of a five-part series that looks at the impact of the Internet of Things (IoT) on society.

    I’m often asked about the value of the IoT — sometimes directly, but often indirectly, as in “How can a deluge of data create value?”

    Let’s look at an example of electric motors in industrial environments and the ways the IoT produces some real value, perhaps in some ways you hadn’t considered.

    Electric motors: The workhorses of industrial life

    Electrical Motors: The workhorses of the industry Electric motors come in all sizes, from very small to very large. They usually run on main power, but sometimes on batteries, like in electric cars. We all have many electric motors in our homes — in our vacuum cleaners, fridges, freezers, garage door openers. And, of course, many toys have miniature electric motors, like the locomotives in model trains.

    Factories are also equipped with many electric motors used for all kinds of jobs: lifting, pressing, pumping, sucking or drying — basically everything that can be done with motion. Electric motors are the workhorses of industry today. They’re also used in areas that are too dusty, dangerous or difficult to reach by human effort. In short, modern industrial life doesn’t exist without the electric motor.
     

    Maintenance, maintenance, maintenance

    Electric motors are mechanical devices, so it’s no surprise that they go down occasionally. Statistics show a failure rate of 7% per year; on average, an electric motor stops working once every 14 years. Not bad, you might think — but for a factory with a hundred electric motors, that means one motor is down just about every month. And keep in mind that one motor going down sometimes means a whole production line going down, which can become very expensive, very quickly. Now factor in the reality that motor failures can come with incredibly unfortunate timing, like just before that critical order has to be delivered.

    Electric motors in the factory: The workhorses of industry todayTo reduce unexpected downtime, factories employ maintenance crews. Maintenance of electric motors is an important part of their efforts, but it’s also expensive. There are several approaches to maintenance:

    • Preventive maintenance. Maintenance schedules are based on an estimate of how long the average electric motor runs. To be on the safe side and avoid complete motor failure, maintenance usually occurs too early (although occasionally too late), and well-functioning parts still in good condition may be replaced. The catch? There’s no guarantee that a new problem won’t occur shortly after maintenance takes place.
    • “Run-to-failure” maintenance. This approach waits to do maintenance until the machine stops working. This typically results in full motor replacement, because repairing a rundown electric motor on the spot usually isn’t simple.
    • Condition-based maintenance. Before electric motors go down, they generally start to show irregularities like noise, imbalance, drag, etc. In a condition-based approach, a maintenance specialist goes to every electric motor and “listens” to it with the appropriate tools, much like a doctor with a stethoscope. Depending on the environment, this may be an easy job or a difficult and even a dangerous one. And, of course, the doctor can't be everywhere at once.

     
    Despite its drawbacks, preventative maintenance is probably better and more cost-effective than the “run-to-failure” alternative — but condition-based may be a better option … especially when you bring in the IoT.
     

    Condition-based maintenance: Made stronger with AI and IoT

    With the IoT, every electric motor on a factory floor is equipped with one or multiple sensors that are connected (preferably wirelessly) to a control database that continuously collects data about the motors. The control database can use artificial intelligence (AI) to learn normal behavior for every motor and then, after a typically short period of learning, it can generate immediate alerts when deviations from that normal occur. In other words, the IoT combined with AI not only sees problems coming, it continuously scans for problems.

    The true value of the IoT: machines with connected sensors for maintenanceKeep in mind that this control database doesn’t need to be programmed. It can simply be fed with data and then learns by itself “automatically” what is normal and what are exceptions. When an exception (i.e., a problem) occurs, it sends an immediate alert, which in many cases avoids total motor failure and replacement. This kind of smart alert also allows the treatment to match the problem at the moment it starts to manifest, rather than general maintenance that may be too early, too late or miss the pending failure completely. Depending on the severity of the problem and alert, the motor’s downtime can even be planned to minimize any disruption to operations.

    Finally, this kind of sensor-based data collection is far more precise and thorough than anything humans could achieve. A slow deterioration of the quality of any given electric motor will continue undetected by human eyes and ears until a serious problem develops or failure occurs, but the IoT will notice even the smallest shifts in normal performance over a longer period of time.
     

    The true value of the IoT: Making better decisions faster

    We think we live in a modern world, but we actually waste a lot of resources and money by making the wrong decisions and/or making decisions too slowly. The promise of the IoT is that we can now collect enough data — cost-effective data that already exists, but that we never captured. And we can capture this data continuously, and quite effortlessly, in enormous volumes. With AI, we can learn from it to make better decisions, faster.

    Back to the original question, then. What value does the IoT bring? It enables people to make better decisions, faster.
     

     

    Did you miss the other posts in our IoT series? Catch up on all of them:

     

    Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.

    Cees Links

    About the Author

    Cees Links
    General Manager, Wireless Connectivity Business Unit

    Cees Links (pronounced "Case") was the founder and CEO of GreenPeak Technologies, acquired by Qorvo in 2016. He is a pioneer of the wireless data industry, a visionary leader bringing the world of mobile computing and continuous networking together. In 2017, he was honored as a Wi-Fi pioneer with the Golden Mousetrap Lifetime Achievement Award by Design News.

    The Impact of the IoT Demystified
    The Impact of the IoT Demystified

    Explore how the Internet of Things will affect society, from jobs to artificial intelligence and more.

    Read the White Paper >
    • Applications
      Internet of Things

      Qorvo's innovative portfolio enables the smart home, smart energy and other IoT applications.

    • Applications
      Smart Energy

      Qorvo's smart energy and Zigbee product offerings cover a wide array of ISM frequency bands from 169 MHz through 2.5 GHz.

    • Applications
      Industrial, Scientific & Medical

      Qorvo's portfolio includes highly integrated FEMs that cover the ISM bands from 169 MHz to 2.5 GHz.

    • Products
      Internet of Things

      Our products for the IoT support ISM, Zigbee, Thread and Bluetooth® bands.