April 20, 2017

    Gallium (Ga) is a chemical element with atomic number 31. Gallium doesn’t exist freely in nature. Instead, it’s a byproduct in the production of zinc and aluminum.

    The GaN compound is formed by gallium and nitrogen atoms arranged, most commonly, in a wurtzite crystal structure. The wurtzite crystal structure (shown in the figure below) is hexagonal and is characterized by two lattice constants (marked a and c in the figure).

    The GaN crystal structure

    The GaN crystal structure

    In the semiconductor world, GaN is usually grown at a high temperature (approximately 1,100°C) by metal organic chemical vapor deposition (MOCVD) or molecular beam epitaxy (MBE) techniques on a foreign substrate (silicon carbide [SiC] for RF applications, or silicon [Si] for power electronics applications).

    The GaN-on-SiC approach combines the high power density capabilities of GaN with the superior thermal conductivity and low RF losses of SiC. That’s why GaN-on-SiC is the combination of choice for high power density RF performance. Today, you can get GaN-on-SiC substrates up to 6 inches in diameter.

    The GaN-on-Si combination has a much poorer thermal performance and higher RF losses but is much cheaper. That’s why GaN-on-Si is the combination of choice for price-sensitive power electronics applications. Today you can get GaN-on-Si substrates up to 8 inches in diameter.

    So why does GaN outperform other semiconductors in RF applications?

    GaN is a relatively new technology compared to other semiconductors, such as Si and GaAs, but it has become the technology of choice for high-RF, power-hungry applications like those required to transmit signals over long distances or at high-end power levels (such as radar, base transceiver stations [BTS], satellite communications, electronic warfare [EW], and so on).

    GaN-on-SiC stands out in RF applications for several reasons:

    1. High breakdown field: Because of GaN’s large bandgap, the GaN material has a high breakdown field, which allows the GaN device to operate at much higher voltages than other semiconductor devices. When subjected to high enough electric fields, the electrons in the semiconductor can acquire enough kinetic energy to break the chemical bond (a process called impact ionization or voltage breakdown). If impact ionization is not controlled, it can degrade the device. Because GaN devices can operate at higher voltages, they can be used in higher-power applications.
    2. High saturation velocity: Electrons on GaN have a high saturation velocity (the velocity of electrons at very high electric fields). When combined with the large charge capability, this means that GaN devices can deliver much higher current density.
       
      The RF power output is the product of the voltage and the current swings, so a higher voltage and current density can produce higher RF power in a practically sized transistor. Simply put, GaN devices can produce much higher power density.
    3. Outstanding thermal properties: GaN-on-SiC devices exhibit outstanding thermal properties, due largely to the high thermal conductivity of SiC. In practical terms, this means that GaN-on-SiC devices don’t get as hot as GaAs or Si devices when dissipating the same power. A “colder” device means a more reliable device.

    To learn more about GaN, including the benefits of GaN’s high power density, download our e-book, GaN RF Technology For Dummies®.

    – Excerpted with permission from John Wiley & Sons, Inc., from GaN RF Technology For Dummies.

    GaN For Dummies® Volume 1

     

    Have another topic that you would like Qorvo experts to cover? Email your suggestions to the Qorvo Blog team and it could be featured in an upcoming post. Please include your contact information in the body of the email.

    Download GaN For Dummies® from Qorvo
    GaN For Dummies®

    Learn about the basic technology of GaN and its applications in RF design.

    Get Your Free e-Book >